Changing Advanced Security Enabled to False - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

About this task

By default, the Advanced Security Enabled attribute on the Site object is set to True for the Metasys system installed at or upgraded to Release 10.0 or later. This attribute provides an improved layer of security between Metasys Site Directors and devices. With this attribute set to true, older methods of secure communication between the Site Director and its network engines are disabled. This means a Site Director at Release 10.0 or later discards all communication attempts from network engines up to Release 10.0. This setting applies to the entire site, so if you have any network engine on the site that is running a Metasys release earlier than Release 10.0, use the steps in this section to change this Site object attribute to False. You can use either SCT (offline method), the Site Management Portal UI (online method) or the Metasys UI (online method). To use the online method, follow these steps:

Procedure

  1. Log on to the Metasys UI of the Site Director.
  2. Open the Site View for the Site Object.
  3. Locate the Advanced Security Enabled attribute under the Operational Data section.
  4. Click the linked value to edit it.
    Figure 1. Changing the Advanced Security Enabled attribute in Metasys UI
    Figure 2. Changing the Advanced Security Enabled attribute in SMP
  5. Click the down arrow and select false.
  6. Click the save icon. The server and engines across the entire site no longer use advanced security.
  7. As an option, use SCT to upload the Site Director so that this change is reflected in the database archive.
    Note: If some time later you change the Advanced Security Enabled attribute from False to True, a user message appears to indicate that all network engines before Release 10.0 are disconnected from the site because they can no longer communicate with the Site Director using advanced security. Do not set Advanced Security Enabled to True until all network engines are upgraded to Release 10.0 or later.