Binding the secure certificate - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

About this task

To bind a secure certificate for a Metasys server or SCT computer:

Procedure

  1. In Control Panel, select System and Security > Administrative Tools and double-click Internet Information Services (IIS) Manager. The IIS main screen appears.
  2. Expand the Connections in the left pane so that Default Web Site appears. Click Default Web Site.
  3. On the Actions pane, click Bindings under Edit Site. The Site Bindings screen appears.
  4. Click Add. The Add Site Bindings screen appears.
  5. Under Type, select https. Under SSL certificate, select the name of the server certificate you imported in Completing a server certificate request. Click OK.
    Note: Make sure that proper certificate revocation, such as Online Certificate Status Protocol (OCSP) stapling, is enabled and configured. For more information about OCSP configuration refer to https://docs.microsoft.com/en-us/openspecs/windows_protocols/ms-ocsp/5792b4c4-c6ba-439a-9c2a-52867d12fb66
  6. If you need to import root and intermediate certificates of the Metasys Server or SCT computer at a client computer, go to Importing root and intermediate certificates. This step is necessary if you want the green shield icon to appear on Metasys SMP and SCT login and user interface screens.

    If you want to skip that step and you want to verify the certificate chain you created in the previous sections, see Verifying the server certificate chain.