Primary requirements - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

The following is a list of requirements for using Active Directory service with the Metasys system at the customer’s site. The steps for setting up Active Directory service are primarily the responsibility of the customer’s IT department. Installation of the Metasys software is usually performed by others, but often supervised by IT personnel. These requirements are based on answers given for the questions posed in Table 1, though not all requirements apply to every installation.