RADIUS and Syslog Configurations - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

RADIUS and Syslog may be configured only online by a Metasys system administrator using the SMP.

Important: If the RADIUS configuration is not restored in the servers or network engines during a download, all previously added RADIUS users do not appear in the users list and remain hidden until RADIUS is enabled.