Supported operating system, SQL Server software, and IIS versions - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

Refer to the literature for the Metasys products you are installing for a list of supported operating system and SQL Server software versions. For an overview of software supported by the Metasys system, refer to the Metasys® Server Installation and Upgrade Instructions (LIT-12012162) , SCT Installation and Upgrade Instructions (LIT-12012067) , Open Application Server Installation and Upgrade Instructions (LIT-12013222) , or the ODS Installation and Upgrade Instructions (LIT-12011945) .

As new software and service packs become available, Johnson Controls tests them for use with Metasys software. Be aware that installing other software or updating the operating system with a new service pack on a computer running Metasys software may adversely affect the system.

The following table lists the versions of IIS that can be used with Metasys products.

Table 1. Supported IIS Versions

Operating System

Supported IIS Version

Windows 7 Professional, Enterprise, and Ultimate Editions with SP1

IIS 7.5

Windows Server 2012 with Update (KB3172614)

IIS 8.0

Windows 8.1 Pro and Enterprise Editions with Update (KB2919355)

Windows Server 2012 R2 with Update (KB2919355)

IIS 8.5

Windows 10 Pro and Enterprise Editions with Creators Update (version 1809 or later)

Windows Server 2016 with Update (KB4489890)

IIS 10.0