Supported network engine models and releases with security attributes - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

The following table lists the latest Metasys system software releases of each network engine model along with the security attributes available for each. As the security features of the Metasys system have improved with each new software release, the network engines have likewise been improved.

Table 1. Network engine release levels

Release with Security Attributes

NCE25

NAE35, NAE45

NAE55, NAE85

NIE29, NIE39, NIE49

NIE59, NIE89

NIE55, NIE85

SNC, SNE

Release 9.0

  • Site Security Level
  • Allow Http

X

X

X

X

X

X

N/A

Release 9.0.7

  • Site Security Level
  • Allow Http

X

X

N/A

X

N/A

N/A

N/A

Release 10.0

  • Site Security Level
  • Allow Http
  • Advanced Security

N/A

N/A

X

N/A

X

X

N/A

Release 10.1

  • Site Security Level
  • Allow Http
  • Advanced Security

N/A

N/A

X

N/A

N/A

N/A

X