Launcher download options and proxy settings - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

You can use an Internet browser to download the Launcher software that the SMP UI requires. To do so, enter its URL in the address field using this format:

http://<Metasys Server or engine computer name>/metasys

One of the following Launcher Download screens appears (Figure 1).

Figure 1. Windows Launcher Download

At Release 10.0 or later, the Launcher Download screen provides one choice (Full Launcher Installer) and at Release 9.0.7, the Launcher Download screen provides two choices (Full Launcher Installer and Single Site Connection), but the Single Site Connection is no longer active.

When you click Full Launcher Installer for a network engine at Release 9.0.7 or later, the browser routes you to the public Launcher download website. Refer to that website for instructions on how to download the Launcher installation file to a location on your computer. When complete, run the Launcher installation. For details, refer to the Launcher Installation Guide (LIT-12011783).

When you click Full Launcher Installer for a Metasys Server at Release 10.0 or later, a security warning screen may appear (Figure 2). This screen gives you the option to Run or Save the Launcher installation file.

Figure 2. File Download - Security Warning Screen

Click Run on the File Download - Security Warning screen. The Internet Explorer - Security Warning screen may appear (Figure 3).

Figure 3. Internet Explorer - Security Warning Screen

For this screen, click Run to allow local installation of the Launcher software. For more details, refer to the Launcher Installation Guide (LIT-12011783).

Launcher Proxy Settings

The full version of the Launcher tool lets you update certain options, including proxy settings (Figure 4).

Figure 4. Application Options Screen

If the building network uses a proxy server for connection to the Internet, click Manual under Proxy Selection and enter the IP address or host name and port number of the proxy server.