Spanning trees - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20

Improperly configured spanning trees cause excessive Spanning Tree Protocol (STP), Rapid Spanning Tree Protocol (RSTP), or Bridge Protocol Data Unit (BPDU) traffic, which causes Metasys network engines to reset. Be sure all spanning trees are properly configured.