The following figure is an example of the connectivity and protocols used in a Metasys system using the OWS or M5 Workstation and NCMs. See Figure 1 with Table 1, and Figure 1 with Table 1, for the full set of protocols used by the engine, Metasys Server, and Site Management Portal UI.
Interaction between Callouts |
Protocol |
Communication Direction |
|
---|---|---|---|
1 |
2 |
N1 |
Bidirectional |
1 |
3 |
SNMP, SNMP Trap |
Unidirectional |
2 |
2 |
N1 |
Bidirectional |
2 |
4 |
N1 |
Bidirectional |