Many-to-one wireless network - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20

The following figure is an example of the connectivity and protocols used in a Metasys network using the Many-to-One Wireless Room Temperature Sensing (WRS) application. The WRS system is supported at Metasys Release 9.0 or earlier.

Figure 1. Metasys System with Many-to-One Wireless Room Temperature Sensing Application (Release 9.0 or earlier)

Table 1. Metasys System with Many-to-One Wireless Room Temperature Sensing Application

Interaction between Callouts

Protocol

Communication Direction

1

2

Tunneling over Ethernet

Bidirectional

2

3

Wireless Many-to-One Sensing (802.15.4)

Bidirectional (2.4 GHz Channelized, 2.4 GHz DSSS Wireless Protocol)

4

2

HTTP

Unidirectional

The WRS Series sensors and WRS receivers operate on the 2.4 GHz Industrial, Scientific, Medical (ISM) band and use multi-frequency DSSS technology. The receiver meets the IEEE 802.15.4 standard for low power, low duty-cycle wireless transmitting systems.

The 802.15.4 standard radio is used for employing control networks within a building. This technology uses 16 different channels, allowing 802.15.4 devices, such as the WRS Series systems, to coexist with 802.11 devices.

The Many-to-One system use two-millisecond multi-frequency redundant data transmissions. The sensor transmits a rapid sequence of high-speed (two millisecond) redundant data bursts to an associated receiver approximately every 60 seconds. The sensor transmits up to five redundant data bursts in rapid sequence, and each burst is transmitted on a different ZigBee frequency. When a single data burst is successfully received and acknowledged (or if all five redundant data bursts fail), the sensor goes dormant for approximately 60 seconds and then repeats the rapid transmission burst sequence.

Multi-frequency, redundant data-transmission sequences greatly enhance the success of the wireless sensing system data transmissions. Transmitting short, high-speed data bursts at 60-second intervals also reduces wireless data transmission collisions and interference with other Wi-Fi transmissions. The DSSS technology virtually eliminates accidental and unauthorized wireless interference.

1 Port 4050 is recommended for the WRS-RTN Receiver.
2 In Unidirectional communication, only the originating device initiates requests (assuming synchronous response is allowed in the request).