Active Directory network - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

The following figure is an example of the connectivity and additional protocols used in a Metasys system that uses Active Directory service. Table 1 describes the protocols used in Figure 1.

Figure 1. Metasys system with Active Directory service