Network Interface Cards (NICs) - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

The Metasys software supports more than one NIC on a computer running Metasys software (including Metasys server, SCT, NxE85, NIE89 and LCS85 software).

Follow the instructions in the appropriate Metasys installation literature to configure the NIC that Metasys software uses. For example, the Interface Metric for the Metasys network card must be set to 1, and all other NICs on the computer set to an Interface Metric higher than 1.