Last login - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20

The main screen of the Metasys server or SCT user interface indicates the last time and date that the user successfully logged in. For enhanced security, only the first three letters of the user's name appear, followed by three asterisks (for example, Use***). If the user has never logged in, Never appears in the Last Login field. (See Figure 1 and Figure 2.)

Important:

To preserve the current configuration for all Metasys system users, including last login time, always upload the device into the SCT before making changes and downloading a database. User configuration information is stored in the Security database. The Security database is restored during a device download. When an older archive is downloaded into the device, the most recent user password, properties, and login time are lost.

Figure 1. User's last login

Figure 2. User never logged in