Changing Remote Desktop settings - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20

About this task

For sites requiring remote access to devices, including Metasys servers, we recommend changing the Remote Settings on the device to allow connections only with Network Level Authentication. Use the following steps to change the setting on the device.

Procedure

  1. On the host computer, go to Control Panel > System > Remote Settings. The System Properties window appears.
  2. In the Remote Desktop section, select Allow connections only from computers running Remote Desktop with Network Level Authentication (more secure).
  3. Click OK.