Metasys Application Programming Interface (API) - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20

Additional enhancements to the Metasys Server software at Release 10.1 include a REST-compliant Metasys Monitoring and Commanding Application Programming Interface (API) that enables reading, writing, and commanding of one or more Metasys objects/properties to provide a secure way to bi-directionally integrate with third-party applications.

This is the latest in a suite of APIs that include the REST-compliant API that enables data to be securely extracted from the Metasys system and integrated with third-party data visualization tools to meet robust data analysis and reporting needs and the Metasys API for the TeleHealth Engagement Application that facilitates reliable two-way communication between the TeleHealth patient engagement application and Metasys system to provide patients direct control over their healthcare space for increased comfort and satisfaction.