Encrypted email - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

Metasys software features an email encryption capability that encrypts user names and passwords as they are entered into the SMP UI. Embedded and server machines can thereby send emails to email servers over a secure channel (secure socket layer [SSL]). The entire email payload is encrypted, and allows Metasys software to communicate to email servers that require SSL connections.

Users can configure email encryption with no authentication required, including SMTP authentication, and POP-Before-SMTP authentication.