DNS implementation considerations - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20

The DNS infrastructure must be configured to do the following:

  • The Metasys server and/or Metasys engine and Metasys DHCP supported devices (TEC20-3C-2 Coordinators, WRS-RTN Many-to-One Receivers) must be defined in the same DNS domain.

  • The Metasys server and/or Metasys engine and Metasys DHCP supported devices (TEC20-3C-2 Coordinators, WRS-RTN Many-to-One Receivers) require that DNS servers be defined to resolve hosts in the domain they are in.

  • If the DNS server and the Metasys server and/or Metasys engine are in different networks (VLANs), routing must be available between networks.