Software supported on Windows Server platforms - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English
  • ADX

  • ODS

  • OAS

  • Metasys Advanced Reporting System

    Note: Metasys Advanced Reporting supports installation on a computer with SQL Server software. However, Energy Essentials reports does not support installation on a computer with SQL Server 2017 or SQL Server 2016.
  • Metasys Database Manager

  • Metasys Export Utility

  • Metasys System Secure Data Access

  • Metasys UI

  • Metasys UI Offline
  • SCT

  • Site Management Portal UI client computer (computer browsing to the Site Management Portal UI)

  • NAE85

  • LCS85

Software and technologies not listed here are not supported. Refer to the appropriate technical literature for the technology that you are using to verify compatibility with Windows Server operating systems.