Internet Explorer enhanced security configuration - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20

This section applies to the web browser on any computer running a supported server-class operating system. By default, Internet Explorer Enhanced Security Configuration is enabled on this operating system. When you start the Internet Explorer web browser, the Internet Explorer Enhanced Security Configuration is enabled message appears (Figure 1).

Figure 1. Internet Explorer Enhanced Security Configuration is Enabled Message

The Internet Explorer Enhanced Security Configuration establishes a configuration for your computer and for the Internet Explorer web browser. This configuration decreases the exposure of your server to potential attacks that may occur through web content and application scripts. As a result, some websites may not display or perform as expected. For example, the Enhanced Security Configuration may prevent the download of the Launcher application.

To disable Enhanced Security Configuration, start Server Manager and select Local Server. Locate the IE Enhanced Security Configuration setting. Click On to open the Internet Explorer Enhanced Security Configuration window. Click Off for administrators and users, as recommended by the IT administrator.