Configuring computer as Application server for use as ADX - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

For information on configuring the computer as an application server, refer to the installation instructions for the Metasys software that you are using (for example, Metasys server or SCT).