Administrator rights - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

Depending on your operating system login privileges, you may need to perform the steps listed in Table 1 to use Metasys software (including logs) or access Windows operating system features and SQL Server software on your Windows Server operating system.

Table 1. Login Privileges and Steps

Login Privileges

Steps to Run Software

Not Logged in as the Windows Account with username of Administrator.

To run the software:
  1. Right-click the software icon on your desktop or software name in a menu.
  2. Select Properties.
  3. Select Run As Administrator.
  4. Click Allow.
Refer to the documentation for the specific Metasys software you are using for more information on how to perform tasks that require Administrator privileges.

Logged in as the Windows Account with the user name of Administrator.

Run the software without additional steps.