Windows scheduled features - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

Some features of Windows 10, Windows 8.1, or Windows 7 should be rescheduled depending on the load for the Metasys server. By default, the Windows Defender security tool scans the operating system at 2 A.M. every day, and the Disk Defragmentation tool runs every Wednesday at 1 A.M. If the Metasys server is busy at these times, you should reschedule the process for a time when the Metasys server is less busy.