Field device offline/online - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

Field devices (for example, FECs and VMAs) are treated the same way as supervisory devices. If the field device has the appropriate alarm extension defined, the controller generates online/offline alarms (Traps) as they occur.