As highlighted in the Trap Examples section, each Trap OID sends the same set of attributes. You
can translate attributes values (evPreviousState) using the key values in the
following table.
Key |
Text |
Key |
Text |
---|---|---|---|
0 |
Normal |
68 |
Alarm |
1 |
Fault |
69 |
Trouble |
2 |
Off Normal |
70 |
Status |
3 |
High Limit |
71 |
Offline |
4 |
Low Limit |
72 |
Shutdown |
64 |
Low Warning |
73 |
Unreliable |
65 |
High Warning |
75 |
Online |
66 |
Low Alarm |
65535 |
Unknown Previous State |
67 |
High Alarm |