Base OID - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

1.3.6.1.4.1.4399.2.1.1.1.1.3.x

where x is an integer that represents the attribute of the point (Table 1).


Table 1. Device Diagnostic Attributes

x

Description

.647

Battery Condition

.650

Change of Value Receives Per Minute

.651

Change of Value Transmits Per Minute

.844

Object Count

.2395

Estimate Flash Available

.2579

CPU Temp (Not Available on NAE-45)

.2580

Board Temperature

.2581

Memory Usage

.2582

Object Memory

.2583

CPU Usage

.2584

Flash Usage

.32565

Pager Dial Status