Configuring trap filtering - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20

Of the available attributes listed in Table 1, configure the NMS interface to filter the attributes to be trapped. You also must select these attributes when you configure the SNMP DDA alarm notifications and destinations in the device object. For details, refer to the NAE Commissioning Guide (LIT-1201519), SNE Commissioning Guide (LIT-12013352), SNC Commissioning Guide (LIT-12013295), Open Application Server (OAS) Commissioning Guide (LIT-12013243) , ODS Commissioning Guide (LIT-12011944) , and the ADS/ADX Commissioning Guide (LIT-1201645). This list applies to Metasys alarm events only.

Table 1. Available Attributes for Trap Filtering

Field Names

ackRequired

eventValue

itemName

eventDetectionTimestamp

evPriority

SiteName

eventMessage

itemCategory

units

eventPreviousStatus

itemDescription

 

eventUniqueIdentifier

itemFullyQualifiedReference