When an object with an alarm extension generates an event in the Metasys system, the SNMP Agent sends the same Alarm Type that was raised in the system (Metasys Server or network engine). Examples include High Warning and Low Alarm. Each Trap OID also sends the attribute values that were selected for the trap (Table 1).