Alarm clear trap - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

When an alarm Return to Normal state occurs, the SNMP Agent reacts in the same manner as when the alarm was raised. In this way, the Alarm situation is cleared with a NormalEvent message.