Agent restart trap - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

When an Agent Restart occurs, a coldstart trap is sent when the supervisory device (NAE, for example) powers on. Table 1 lists the attributes that are sent.

Table 1. Attributes for Coldstart Trap

Attribute Names

hostName

ipAddress

macAddress

subnetMask