Three Johnson Controls® MIB files are provided on the product media and on the Metasys system website for download (Table 1). The NMS software can read these MIB files, as well as the standard MIB files.
Johnson Controls MIB Files |
Standard MIB Files 1 |
|||
---|---|---|---|---|
jcicontrolsgroup.mi2 |
SNMPV2_MIB.mib |
|||
johnsoncontrolsinc.mi2 |
SNMPV2_SMI.mib |
|||
msea.mi2 |
SNMPV2_TC.mib |
These MIB files define the data available from the Metasys SNMP feature. They provide the OIDs that describe the traps and point types available in the Metasys system. For example, an OID is available to describe the alarm state of a point. Loading the MIB files into the NMS provides translation of the Metasys data.
1 Standard MIB files are available on the Internet.