User Account in Active Directory Service - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20

A login account assigned to a user that is created, stored, and maintained only within Active Directory service; this User Account provides access to Active Directory service Network Resources. It may also provide access to the Metasys system when added and privileged using the Metasys Security Administrator System.