Transport Layer Security (TLS) and Secure Sockets Layer (SSL) - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

Transport Layer Security (TLS) is the successor to the Secure Sockets Layer (SSL) protocol. Both communication protocols provide network security to client-server applications.

For general information on how to implement TLS or SSL, refer to https://technet.microsoft.com/en-us/library/cc784450(v=ws.10).aspx.

The Metasys software can use Secure Channel and built-in implementation of TLS or SSL included with the Microsoft Windows operating system. For more information about Secure Channel, refer to https://msdn.microsoft.com/en-us/library/windows/desktop/aa380123(v=vs.85).aspx.