Simple Network Time Protocol (SNTP) - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20

A simplified version of NTP. These protocols allow one computer to ask another computer what time it is across a TCP/IP network, then set its own clock accordingly. A number of public Simple Network Time Protocol (SNTP) time servers keep track of time with a very high degree of accuracy that can be used to ensure that the Site Director is synced to real time. You can find lists of public SNTP time servers by performing a search on the Internet.