Service Account in Active Directory Service - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20

A login account assigned to an application to enable the application to perform privileged actions within Active Directory service; the Metasys system requires one or more Service Accounts to be assigned to allow the system to perform directory queries and request Active Directory service authentication. Only one Service Account is allowed per domain.