Remote Authentication Dial-In User Service (RADIUS) - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20

Remote Authentication Dial-In User Service (RADIUS) is a network protocol that provides centralized authentication. RADIUS is a client/server protocol, running on the application layer, that uses TCP or UDP which provide host-to-host communication for applications. RADIUS is used by the server and network engines to authenticate the identity of authorized non-local users of the Metasys system.