Organizational Units (OU) - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20

A container within Active Directory service that should be used to reflect the details of the organization’s business structure or to delegate administrative control over smaller groups of users, groups, and resources. An organizational unit (OU) inherits security policies from the parent domain and parent OU unless it is specifically disabled.