Domain Name System (DNS) - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

The method by which host domain names are translated into IP addresses. A domain name is a meaningful and easy-to-remember handle for an Internet address. DNS is the Internet standard for naming host devices and mapping host names to IP addresses.