Active Directory Service Schema - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20

The formal definition of all object and attribute data that can be stored in the directory; for example, user is an object type with attribute data of name, first name, last name, email, and so on. The schema is made up of object classes and attributes. The base (or default) schema contains a rich set of object classes and attributes to meet the needs of most organizations, and is modeled after the ISO X.500 standard for services.