Microsoft SQL Server licensing requirements - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

All versions of Microsoft SQL Server Standard or Enterprise software use a per core licensing model. The SQL Server Express versions, however, do not require licensing. To determine the licensing needs for SQL Server Standard or Enterprise software that is installed on a Metasys Server:

  • count the number of cores in the processor
  • purchase the adequate number of core licenses

To assist you in counting the number of processor cores, refer to the specifications provided by the computer manufacturer or download the free Microsoft Assessment and Planning Toolkit ( https://www.microsoft.com/en-us/download/details.aspx?id=7826). This toolkit may require the assistance from an IT professional. You may also consult the Microsoft Core Factor Table available at http://go.microsoft.com/fwlink/?LinkID=229882.

After you determine the number of processor cores, purchase the appropriate number of core licenses to allow the ADX computer to access the SQL Server database. If the ADX computer running SQL Server software has multiple cores in the processor, purchase one license for each physical core in the processor. For example, if the computer has a single quad-core processor, purchase four core licenses.

For a split ADX without the Metasys Advanced Reporting System, SQL Server software is installed only on the database server. You must purchase one core license for each physical core in the processor of the database server.

For a split ADX with the Metasys Advanced Reporting System, the database engine component of SQL Server software is present on the database server, and the reporting services component of SQL Server software is installed on the web/application server. You must purchase one core license for each physical core in the processor for both the database server and the web/application server.

Table 1 lists the number of core licenses required based on the number of physical cores in the processor.

Table 1. SQL Server license requirements

Physical Cores in the Processor

Core Licenses Required

(SQL Server Standard/Enterprise software requires a minimum of four core licenses, even for processors with less than four cores.)

1

4

2

4

4

4

6

6

8

8