Completing a server certificate request - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20

About this task

To complete a certificate request for a Metasys server or SCT computer:

Procedure

  1. In Control Panel, select System and Security > Administrative Tools and double-click Internet Information Services (IIS) Manager. The IIS main screen appears.
  2. Under the IIS section in the middle pane, double-click Server Certificates. The Server Certificates panel appears.
  3. On the Actions pane, click Complete Certificate Request. The Specify Certificate Authority Response screen appears.
  4. Use the browse button to locate the certificate that your IT department provided. Specify a friendly name for the server. Select Personal under Select a certificate store for the new certificate if this field appears. Click OK to complete the certificate request. The Server Certificates window appears indicating the new certificate has been imported.
  5. Next, you need to bind the certificate. See Binding the secure certificate.