Additional requirements - Metasys - LIT-12011279 - General System Information - Metasys System - 10.1

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
10.1
Revision date
2019-12-20
Language
English

The following are additional requirements:

  • Obtain the fully qualified domain names for all domains that are to contain Metasys system users. The name must be the domain level (and not the forest level or some other level).

Note: This information is necessary at the time when Active Directory service users are added to the Metasys system with the Security Administrator System tool. For details, see User account rules.
  • Obtain the corresponding pre-Windows 2000 domain names (short format of the domain name). This information is useful because the Metasys system user can specify this format at the login screen of the Site Management Portal UI.

For additional requirements, see Service account.