Field value attribute - Metasys - LIT-12013150 - System Integration - Modbus Vendor Integration - 10.1 - 9.0.7

Network Engine Commissioning for Modbus Vendor Integration Application Note

Product
Building Automation Systems > Utilities and Integrations > Modbus Vendor Integration
Document number
LIT-12013150
Version
10.1
9.0.7
Revision date
2021-03-03

Using the integration, you can read the value of data coming directly from the integrated device. This information is stored in the Field Value attribute on the Hardware tab of the object. See Figure 1. The string contains the register or coil address of the point and the value in hexadecimal or binary format.

Figure 1. Object hardware tab

Figure 2 shows an example of a field value error message from the device. Use the information from the Field Value attribute to help you correct the error.

Figure 2. Error message from device