The network engines are Ethernet-based, supervisory engines that connect Building Automation System (BAS) networks to IP networks. You can monitor and control BAS field devices from a computer using the Launcher application. Install Launcher version 1.7 on your computer. Refer to the Launcher Installation Instructions (LIT-12011783) .
The SNC combines the network supervisor capabilities and IP network connectivity of SNE network engines with the Input/Output (I/O) point connectivity and direct digital control capabilities of equipment controllers. The network engines provide scheduling, alarm and event management, trending, energy management, data exchange, and password protection.