Note: Two Modbus trunks or 1
Modbus and 1 M-Bus integrations are supported
Figure 1 shows how different NxE models and devices are configured in Modbus integrations that use RTU and TCP communication.
Figure 1. Devices connected to an NAE55 and NAE85 through Modbus
RTU and Modbus TCP

Figure 2 show another example using an NxE models and devices with Modbus integrations.
Figure 2. Devices connected to an NAE35 or NAE45 through two
Modbus RTU integrations

Figure 3. Devices connected to an SNC through Modbus
RTU