Summary of changes - Metasys - LIT-12013150 - System Integration - Modbus Vendor Integration - 10.1 - 9.0.7

Network Engine Commissioning for Modbus Vendor Integration Application Note

Product
Building Automation Systems > Utilities and Integrations > Modbus Vendor Integration
Document type
Application Note
Document number
LIT-12013150
Version
10.1
9.0.7
Revision date
2021-03-03

The following information is new or revised:

  • The SNE Series of network engines and the SNC Series of network control engines are new at Release 10.1. Information has been added throughout this document where relevant on the SNEs and SNCs.