Introduction - Metasys - LIT-12013150 - System Integration - Modbus Vendor Integration - 10.1 - 9.0.7

Network Engine Commissioning for Modbus Vendor Integration Application Note

Brand
Metasys
Product name
Modbus Vendor Integration
Document type
Application Note
Document number
LIT-12013150
Version
10.1
9.0.7
Revision date
2021-03-03
Language
English

This document describes how to commission a Network Automation Engine (NAE), a Network Integration Engine (NIE), an SNE, or an SNC Modbus® Remote Terminal Unit (RTU) or TCP vendor integration. It also describes how to upgrade an NIE29, NIE39, or NIE49 at Release 9.0 with integrations to Release 9.0.7, and an NIE59 at Release 9.0 with integrations to Release 10.1.

Note: You can also commission an LCS85 server to use the Modbus protocol. The steps are identical to those described in this document, with the selection of an LCS85 instead of an NAE or NIE as the primary difference. Where reference is made to an NAE85, the information is also valid for an LCS85.
Note: There are no modifications required when you upgrade from Release 10.0 to Release 10.1.

This document does not describe how to mount, wire, or power on an NAE, SNE, or SNC, how to build or download an archive database for a Metasys system site, or how to configure an NAE, SNE, or SNC to monitor and control a Building Automation System (BAS).