Detailed procedures - Metasys - LIT-12013150 - System Integration - Modbus Vendor Integration - 10.1 - 9.0.7

Network Engine Commissioning for Modbus Vendor Integration Application Note

Product
Building Automation Systems > Utilities and Integrations > Modbus Vendor Integration
Document type
Application Note
Document number
LIT-12013150
Version
10.1
9.0.7
Revision date
2021-03-03

Use the Metasys Site Management Portal (SMP) and SCT 13.2 to commission the network engine at Release 10.1. You must have Metasys administrator rights in order to perform the operations detailed in this section.

Important: If you want to upgrade an NIE89 from Release 9.0 to 10.0, you need to backup the System Configuration Tool (SCT) archive, uninstall the NIE89, install the NAE85, and re-configure the integrations from the old NIE89.
Note: The NAE85 does not support a serial interface connection.