Serial port capture - Metasys - LIT-12013148 - System Integration - KNX Vendor Integration - 13.0

Network Engine Commissioning for KNX Vendor Integration Application Note

Product
Building Automation Systems > Utilities and Integrations > KNX Vendor Integration
Document number
LIT-12013148
Version
13.0
Revision date
2023-10-18

About this task

Note: The NAE85 model does not support diagnostic mode at the serial port. Use the USB drive capture method instead.
Note: The SNE and SNC do not have a built in RS-232 interface. To enable RS-232 communication, use a ACC-USBRS232-0 or ACC-USBRS485-0. Refer to SNE/SNC Product Bulletin (LIT-12013296) for ordering information.

Procedure

  1. To activate diagnostic mode, connect a null modem cable between the computer's serial port and the NxE port (RS232C A or RS232C B), or connect the certified ACC-USBRS232-0 USB-to-RS-232 adapter to the SNE or SNC and then connect a null modem cable between the computer's serial port and the adapter.
  2. Start a compatible serial communication program on the computer, for example, HyperTerminal or PuTTY. Configure the communication settings for the diagnostic messages according to the values in Table 1.
    Table 1. Diagnostic port settings
    Identifier Available for Connection Comment
    0

    All models

    - No serial diagnostic output
    1

    All NxE models

    SNExxxxx

    SNCxxxxx

    RS-232C (A)

    First USB-to-RS232 adapter

    First USB-to-RS232 adapter

    Communication parameters:

    115200 bits per second

    8 data bits

    no parity

    1 stop bit

    You can only use the ports if they are not used for serial communication with third party equipment.

    2

    NxE3xxx

    NxE4xxx

    NxE5xxx

    SNExxxxx

    SNCxxxxx

    RS-232C (B)

    RS-232C (B)

    RS-232C (B)

    Second USB-to-RS232 adapter

    Second USB-to-RS232 adapter

    3

    NxE3xxx

    NxE4xxx

    NxE5xxx

    SNExxxxx

    SNCxxxxx

    FC Bus

    FC Bus

    FC Bus A

    FC Bus A

    FC Bus

    4

    NCE251x

    NIE291x

    NxE5xxx

    SNE2xxxx

    FC Bus

    FC Bus

    FC Bus B

    FC Bus B

    7 SNExxxxx, SNCxxxxx First USB to RS-485 adapter1 -
    8 SNExxxxx, SNCxxxxx Second USB to RS-485 adapter2
  3. Select the KNX Integration object and click the Hardware tab.
  4. Click the link in the Vendor Configuration Data field to edit the parameter list:
    • Set parameter 1 to Y.
    • Specify parameter 2 as in Table 1.
  5. Click SAVE.
  6. Capture data for approximately 10 minutes, then disable diagnostic mode by opening the Vendor Configuration Data parameter list again. Set parameter 1 to N and save the change.
  7. Save the captured log as a text file.
  8. Disconnect the cable from the serial port on the NxE or from the serial USB adapter on the SNE or SNC.
  9. Use a text editor to review the log file. The log file includes all the information related to the integration and communication traffic in hexadecimal format.
1 connected first to the engine regardless of USB port used
2 connected secondly to the engine regardless of USB port used