Modifying integration parameters - Metasys - LIT-12013148 - System Integration - KNX Vendor Integration - 13.0

Network Engine Commissioning for KNX Vendor Integration Application Note

Product
Building Automation Systems > Utilities and Integrations > KNX Vendor Integration
Document number
LIT-12013148
Version
13.0
Revision date
2023-10-18

Procedure

  1. Use a web browser to log on to the network engine's UI. Navigate to https://[host name]/UI, where [host name] is the host name or IP address of the network engine.
  2. Select the OPCUA Integration object and click the Hardware tab.
  3. Click the link in the Vendor Configuration Data field to modify the appropriate parameters according to Table 1.
  4. Click SAVE.
    Table 1. VND integration parameters

    Parameter

    Value

    [1]

    Represents whether to capture the KNX driver operations to display the traffic on a serial communication port (Y = enable log; N = disable log).

    If the parameter is set to Y:
    • For the NCE25, NAE35, NAE45, NAE55, NIE59, diagnostic messages are received and can be captured by the use of a serial terminal program.
    • For the SNE and SNC, diagnostic messages are received and can be captured by the use of a serial terminal program.
    • For the NAE85, log files are captured at the USB port.
      Note: For NAE85 and OAS, if you use a USB drive, insert the drive before you enable log capture and remove the USB drive after you disable the log.

    [2]

    Represents the Diagnostic destination where diagnostic details are sent when parameter 1 is set to Y.

    When set to 0, no destination is defined.

    For Ethernet destination, the format of this parameter is <IPv4 address>:<UDP port number>.

    For serial port identifiers see Table 1.

    [3]

    Only the NAE85 and OAS support a USB destination.

    For an NAE85, you must enter the letter of the USB drive.

    [4]

    Not used in this integration.

    [5]

    Represents the timeout, in milliseconds, used to check for offline devices. If a device does not communicate within the timeout period, the integration driver attempts to reconnect with the device.

    [6]

    Represents whether to activate an additional internal log file for use in debugging. Set this parameter to N. If you need to enable additional logging, contact technical support.