Inserting a field device manually - Metasys - LIT-12013148 - System Integration - KNX Vendor Integration - 13.0

Network Engine Commissioning for KNX Vendor Integration Application Note

Product
Building Automation Systems > Utilities and Integrations > KNX Vendor Integration
Document number
LIT-12013148
Version
13.0
Revision date
2023-10-18

About this task

Important: Each KNX IP Gateway has its own unique IP address. Specify the IP address only once for the network engine.

Procedure

  1. Use a web browser to log on to the network engine's UI.
  2. Select the KNX Integration object in the Network Tree.
  3. Click the + icon (Add Network Item) to create the item.
  4. In the Create Item wizard, select Field Device from the General Type drop-down and select Manual.
  5. Select VND Controller from the Object Type drop-down.
  6. Review the unique identifier in the Unique Identifier field and change it.
  7. Click NEXT.
  8. Click CREATE.